Is there a way to attach 0U PDUs to a NetShelter 2-post rack?
Issue:
A customer wants to use a 0U PDU with a NetShelter 2-post rack.

Product Line:
NetShelter 2-post racks

Environment:
AR201

Cause:
The 2-post rack doesn't have an accessory to attach to the side and hand 0U PDUs.

Resolution:
AR7711 is a pair of accessory mounting brackets that can attach to the 2-post rack and bring the PDUs to the side or rear. The User Manual shows several ways to attach the bracket to racks and cabinets.
The AR7711 can hold up to two PDUs.

Schneider Electric Україна

Досліджуйте більше
Серія:
Статті, які можуть бути корисними
Досліджуйте більше
Серія: