Can a trough and partition be installed atop the NetShelter SX cabinet when using VED Kits?
Issue:
Customers choosing cabinets for VED Kits need to know if they can also install troughs and partitions atop the cabinets.

Product Line:
NetShelter SX

Environment:
All models, all serial numbers.

Cause:
It's uncertain if there's room for troughs and partitions when also installing a VED on a cabinet.

Resolution:

See attached file

Schneider Electric Україна

Вкладення
20180508 VED Trough and Partition Installation on Various Depth Cabinets.pdf [54.3 KB]
Досліджуйте більше
Серія:
Статті, які можуть бути корисними
Досліджуйте більше
Серія: