Чим ми можемо вам допомогти сьогодні?

Unity Pro: Get incoherent Output values using mathematics EFs

This is true from Unity Pro V8.0 and will be corrected in Unity Pro V14.0
Each and every condition must be met to have such issue and so occurrence is very low.

This happens if:
The Enable implicit type conversion is checked (Tools/Project Settings/Program/Languages/Common)
The FBD programming language is used.
A Link is used between two EFs.
Source data type of the link and destination data type of the link are different.

None HF is scheduled but unchecking the option Enable implicit type conversion will solve the issue.
In this case thanks to take into account the following NOTICE extracted from Unity Pro documentation: