Issue
Can not connect using Unity Pro or Control Expert.
Product line
M580, M340
Resolution
The most common reason for this behavior is an unterminated bus. If the XBE module is installed, it must be fully terminated. This means that it should have both ports connected. The top port of the XBE in the main backplane should have a terminator marked 'A' on it. The bottom port should have an extension cable connected to the top port of the XBE on the expansion backplane. The bottom port of the XBE in the expansion backplane should have a terminator marked 'B' on it. If any of these four ports is disconnected from either the terminator or cable, the CPU will crash. Even if the expanded backplane is powered down, the cables and terminators must remain in place.
If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.
If you are not located in North America, please contact your local Customer Care Center for assistance:
Опубліковано для:Schneider Electric Україна