Issue:
Number of STO inputs are on the ATV320 drives.
Product Line:
ATV320
Environment:
STO inputs
Cause:
n/a
Resolution:
This drive only has 1 STO input. Could use a logic ( Digital) input and program it for nst and it would work like a STO, but would not be rated, like the STO input.
Опубліковано для:Schneider Electric Україна