Issue:
How can you convert a somove file with an ATV660 over to an ATV630 file?
Product Line:
ATV660, ATV680, ATV960, ATV980, ATV630 and ATV930
Environment:
All
Cause:
Files are not compatible across product families.
Resolution:
It’s not possible to do so. It’s not possible to select another “range” of ATV600. So no you can not convert an ATV660 file over to an ATV630 Drive using somove.
Once you log into Somove and choose topology these ATV660 and other ATV6XX family options will be grayed out.
Опубліковано для:Schneider Electric Україна