Чим ми можемо вам допомогти сьогодні?

How to provide the OFS Manager Log file in Verbose mode ?

  • OFS in verbose mode
To get the most information regarding logs, we need to have the system in verbose mode.
If the OFS DA is not yet in verbose mode, you can check the verbose mode from the OFS Server windows : click on the menu “Misc” and check if “Verbose mode” is checked.

verbose mode
  • Connect OFS Manager to the server
Start “OFS Manager”, once opened click on “server” menu and then click on “connect”

Connect OFS Manager
  • Save the log from OFS Manager:

save log