Чим ми можемо вам допомогти сьогодні?

How do I get the standby CPU to run automatically after program transfer?

Issue

Automatically run standby CPU after the transfer of the program

Product Line

M580

Environment

EcoStruxure Control Expert

Resolution

To have the standby CPU run automatically after a transfer, you need to set the CMD_RUN_AFTER_TRANSFER bit before you transfer to the standby controller. You can set this in an animation table, or you could hard-code this bit to always be true in your first section of logic.