Чим ми можемо вам допомогти сьогодні?

P3 IEC61850 LN value update failure

Issue
After IEC61850 configuration in P3 relay, customer found that some LN was not updating the actual value.
1
_____________________________________________________________
Product Line

Easergy P3 relay
_____________________________________________________________

Environment
All firmware version
_____________________________________________________________
Root Cause
Customer didn’t enable the “Event ON/OFF” which is related to the LN, so the change in value is not updated to LN.
2

3 4
_____________________________________________________________
Solution
1- If our customer want to use some LNs in P3 relay, especially for GGIO LNs, customer should enable separate “Event ON/OFF” function as shown below.
ItemLN(example)Event ON/OFF
Digital input115
Logical output126
Protection137
Virtual input148


2- It will be updated to the manual in future release.
_____________________________________________________________





=====End of document=====