Is the IG2000CBM the same as IG2000CBMPM
Issue:
Is the IG2000CBM the same as IG2000CBMPM
Product Line:
Medical Products
Environment:
IG2000CBM
Cause:
N/A
Resolution:
The IG2000CBMPM is a variation of the IG2000CBM that is designed for mounting in Square-D panels with no back box required. See below for the IG2000CBM part numbers.
Опубліковано для: Schneider Electric Україна