Чим ми можемо вам допомогти сьогодні?

Why does my EEH CSV export include an extra day?

Issue Description:

In Energy Hub> Energy Tab, select an asset, and provide a custom date range, i.e., March 01, 2025 to March 24, 2025. Then click on the "Export all usage data as CSV file"
Export CSV

Note that on the exported CSV file shows:

  • Start time(local timezone): 2025-03-01  12:00:00 AM
  • End time (local timezone) : 2025-03-25  12:00:00 AM

Question: Why does my CSV export include an extra day?

Product Line: Energy Hub

Cause:

When exporting data from the EEH Energy tab, the selected date range is start date inclusive and end date exclusive. For example, if you select March 1 to March 24, the export will include data from March 1. 2025 00:00:00 to March 24, 2025 23:59:59. This means March 25 data is not included in the export.

StartEndTime