Чим ми можемо вам допомогти сьогодні?

How to use "Short Pulse" and "Long Pulse" command on BMXNOR0200H RTU module ?

Issue:

How to use "Short Pulse" and "Long Pulse" command on BMXNOR0200H RTU module ?

Product Line:

BMXNOR0200H RTU module.

Environment:

EcoStruxure Control Expert, Windows 10

Resolution:

To use the Short Pulse command, ensure that the same variable type (C_SC) is configured on both client and server side, with identical IOA settings.

Additionally, the pulse duration must be defined on the server.

EXAMPLE: Using 2 BMXNOR0200H modules:

  • Server IP: 192.168.30.1
  • Client IP: 192.168.30.2

We will configure a variable on both the server and client side, with "Type Identification" set to C_SC and "IOA" set to 2.

On the server, the "Short Pulse" duration will be configured to 100 ms.

SERVER:

Screenshot1

Screenshot2

CLIENT:

Screenshot3

Using a configuration where both the client and server variables are set with Type Identification = C_SC and IOA = 2, and the server's 'Short Pulse' duration is configured to 100 ms:
When the client variable command1.Value changes from 3 to 1, the server variable commande_server.Value will activate for 100 ms, then automatically return to its initial state.

Screenshot4

A network capture performed with the Wireshark tool confirms the communication exchanges between the server and the client :

Screenshot5

This behavior can be validated using the Trend tool in EcoStruxure Control Expert, which provides a visual confirmation of the temporary change in the server variable:

Capture 7

Details of the command to be send:

The example below using "Command.Value" variable:

  • To send a command, we need to trigger the value of the low byte (8 bits) of the %MW register.
  • The value to be transmitted is the value of the lowest bit of this %MW register :

capture10

The point size of C_SC_NA point is 1 bit, as detailed below :

capture20

The command result will be available in the "Command.Status" variable. For more details regardins its different values and their corresponding description, please refer to page 265 of the user manual:

Capture30