An NS MCCB Fuseboard is designed for indoor use only (IP2X, BSEN 60529) and may be transformer, wall or floor mounted. It is suitable for either top or bottom cable entry.
Our Brands
Welcome to the Schneider Electric Website
Discuss this topic with experts