Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the AC-2 rating of the contactor used for load shedding?
Contactors used in load shedding feeder pillars to MOD specification 039 are selected in accordance with the following, to be rated category AC-2:
- RATING, TYPE, OPERATING CYCLES
400A LC1-330 520,000 and 630A LC1-500 480,000

Schneider Electric UK

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and contact centre