How can we help you today?

Is an I-line panelboard that uses a backfed branch breaker as the main breaker suitable for use as Service Entrance?

Issue:
In an I-line panelboard, branch breakers can be used as backfed main breakers in order to feed the interior bus.  Is this application of the I-line panelboard suitable for use as Service Equipment?

Product Line:
Panelboards

Environment:
I-line Panelboards with Backfed Main Breakers

Resolution:
Yes, but the backfed main breaker MUST be labeled as "Main Breaker" for the panel to be rated as suitable for use as Service Entrance.  All panelboards contain a statement on the wiring and torque label indicating the panel can be used as Service Entrance Equipment when applied in accordance with NEC.

Schneider Electric USA
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
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Tech Support: 877-342-5173
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Software and Firmware
  • Product Selector
  • Product Replacement
  • DigestPLUS Online Catalogue
  • Blog
  • Events
  • Schneider Electric Community
  • Sustainability
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings