Issue:
NEMA Size 5 replacement power lugs
Product Line:
NEMA and Definite Purpose Contactors and Starters
Environment:
Type S NEMA Size 5 8502/8536
Resolution:
Depends on Series; select from below:
Series A - Line and Load side lug is part number 25050-44806.
Series B - Line side lug is part number 25050-44806, load side lug is part number 31102-081-01.
NEMA Size 5 replacement power lugs
Product Line:
NEMA and Definite Purpose Contactors and Starters
Environment:
Type S NEMA Size 5 8502/8536
Resolution:
Depends on Series; select from below:
Series A - Line and Load side lug is part number 25050-44806.
Series B - Line side lug is part number 25050-44806, load side lug is part number 31102-081-01.
Released for:Schneider Electric USA