Issue:
8536SBO2S2V02 Description
Product Line:
NEMA and Definite Purpose Contactors and Starters
Environment:
Type S Special NEMA Starters
Resolution:
Special 3 phase starter used in Class 8941duplex controllers. It uses melting alloy overloads.
It is a standard 3 phase starter with the following electrical interlocks mounted and is identified as the ``M2`` starter:
Left side (external) = 9999SX9 & 9999SX10 (overlapping set)
Right side top (external) = 9999SX6 (N.O.)
Right side bottom (internal) = 9999SX12 (N.C.)
8536SBO2S2V02 Description
Product Line:
NEMA and Definite Purpose Contactors and Starters
Environment:
Type S Special NEMA Starters
Resolution:
Special 3 phase starter used in Class 8941duplex controllers. It uses melting alloy overloads.
It is a standard 3 phase starter with the following electrical interlocks mounted and is identified as the ``M2`` starter:
Left side (external) = 9999SX9 & 9999SX10 (overlapping set)
Right side top (external) = 9999SX6 (N.O.)
Right side bottom (internal) = 9999SX12 (N.C.)
Released for:Schneider Electric USA