How can an external error input (run‑permissive) be programmed on the ATS480 soft starter?
First, set your Access Level to Standard or Expert in Menu 10: My Preferences so all necessary configuration options are visible.
Next, navigate through the keypad or SoMove using the following path:
[Complete settings] (CST-)
→ [Error/Warning handling] (CSH-)
→ [External error] (ETF-)
Under External Error Assign (EtF), select the digital input where your permissive signal is wired (for example, DI3).
Make sure the active state is configured correctly—verify whether your permissive is wired for active low or active high, and adjust the setting accordingly.
If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team
If you are not located in North America, please contact your local Customer Care Center for assistance: