Daughters of Mary key figures
$1.3 million in energy cost savings over the next 20 years
24/7 power operation with zero downtime
Up to 1,300 metric tons of CO2 reduced per year
Just as Daughters of Mary of the Immaculate Conception is unwavering in its commitment to caring for the community it serves, so too is the energy that fuels its mission. With a solar powered microgrid system monitored by EcoStruxure Microgrid Solutions, critical care facilities stay up and running while energy costs and the campus’s carbon footprint decrease.
The Challenge
When mounting utility expenses began to impede its mission, Daughters of Mary knew it needed a substantial overhaul of its energy systems. The ideal solution would provide energy cost savings plus maximum efficiency and zero downtime to four separate critical care facilities.
The Solution
A custom solar-powered microgrid system was designed to serve all four buildings, allowing them to operate collectively or individually in grid-tied or island mode. Citizens Energy Corporation, which helped fund the project, manages it through an Energy-as-a-Service agreement using EcoStruxure Microgrid Advisor, Ecostruxure Microgrid Operation, and Energy Control Centers for monitoring and control.
The Results
Now and well into the future, Daughters of Mary can focus on caring for the community instead of worrying about energy costs and downtime. The EcoStruxure platform provides monitoring and control over energy usage for maximum efficiency and cost savings. When it’s not grid-tied, the microgrid system can provide electricity to the critical facilities around the clock.
Steve Bern, Director of Resiliency, Citizens Energy Corporation
Customer testimonial
“We access EcoStruxure on a daily basis when we're reviewing solar production, battery charge and discharge, state of charge, utility import, export, checking building demands. All of the Schneider Electric equipment that's on-site allows us the ability to see exactly what's going on.”
Offers used by Daughters of Mary
Discover EcoStruxure
Learn moreSee all customer stories
Customer success stories