Hôm nay chúng tôi có thể giúp gì cho bạn?

Quantum 984 ladder logic function block execution times

Issue
Quantum 984 ladder logic function block execution times

Product Line
All versions of ProWORX 32

Environment
Windows 7

Resolution
The following tables provide the list of execution times for the 984 ladder logic function blocks.
used in the low end (186 based cpu) and high end (486 based cpu) Quantum PLC's.
axzdfg

sadt
we

ytui
qwe
qwe56

qewrt
re
wqeartyui

AREY
DS
aSDFGH

aserty
asrh
ASDRTY

asrtyu
sdftyu
sadrtyu