Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
Partial reads cannot be performed from a 984-xxx non E PLC

Issue
Partial reads cannot be performed from a 984-xxx non E PLC

Product Line
'ProwORX 32 version 2.1, SP1A

Environment
Windows 7

Resolution
If you try to perform a partial read from a non E 984 PLC (i.e., 984-685, 984-785, etc.) the options for
configuration and logic will be greyed out.

The reason a partial read cannot be performed from a non-E controller is because when the upload
is performed, the configuration automatically gets wiped out from the offline program and replaced with
the uploaded one (Modsoft asks if the user wants to continue before wiping out the configuration).
'ProWORX 32' automatically assumes that the user wants to wipe out the configuration. When this
happens, it causes a mismatch between the offline program and the program that is in the PLC and greys
out the selections.