Hôm nay chúng tôi có thể giúp gì cho bạn?

What is recommended control cable specifications to be used for PLC terminals ?

TeSys Giga contactors are always supplied with push-in type control terminals. Both control voltage (A1-A2) and PLC inputs (X1-X2-X3) terminals can be connected with flexible cables with cable end and solid cables without cables ends.

image.png