Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
Will upgrading the firmware on an APC PDU cause loss of power to the outlets?

Issue:
Will the firmware upgrade process on my APC PDU cause the unit to stop supplying power to its outlets?

Product Line:
APC Rack PDU - AP7***B, AP8*** and APDU9***


Cause:
As long as the PDU is operating normally and there are no active alarms, a firmware upgrade of the management interface will not power on/off any attached loads.
The network management card will reboot during the process, but this will not affect the attached load.