Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
Unable to access ATS web interface via HTTPS

Article available in these languages: Tiếng Pháp

Problem:
Users are not able to access the HTTPS web interface of an AP44xxA Automatic Transfer Switch. May receive warnings of invalid certificates

Environment:
AP44xxA Automatic Transfer Switches with an embedded NMC3

Solution:
The default certificate that is preconfigured on the NMC may have an invalid date, which will prevent users from accessing the HTTPS web interface. Users unable to web can log into the ATS using the provided serial cable, and enable HTTP to web in.

After logging in via HTTP, delete the previous certificate by navigating to Configuration --> Network --> Web --> SSL Certificate, and selecting the "Remove" selection, then click apply.