Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
What is the part number for the Sepam 1000 + Configuration Software?

SFT2841KIT-contains a custom cable (CCA783) for connecting from a laptop pc to the front port of the relays to obtain info, download waveforms, and input configuration and protection settings.
Image1

Original article#3632
Re-published to revised security level: 17 June 2008 by DRM

Applies To:

Public

All content © 1992-2008 Schneider Electric


Legacy KB System (APS) Data: RESL184501 V2.0, Originally authored by DaMi on 06/15/2007, Last Edited by DaMi on 06/18/2008
Related ranges: Sepam 1000, SFT 2841 - SFT2848 (Sepam series 20, 40, 80 software)