Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
Need to know what type of coating should be applied to connectors to avoid corrosion
Issue
Need to know what type of coating should be applied to connectors to avoid corrosion.

Product Line
M340, M580

Environment
N/A

Resolution
To protect connector contacts on our product that are used in harsh enviroments we provide a NyoGel 760 grease for this application.  This product is available from the manufacturer, Nye Lubricants.