Veelgestelde vragen (FAQ's) zoeken
What are the MTBF values for the ABL4 range?
Please note - the ABL4 range is now obsolete and has been replaced by the ABL8 range
These figures are the same for all references in the ABL4 range
MTBF according to standard SN29500 is >500000 hours
MTBF according to MIL Std HDBK217F is >150000 hours
These figures are the same for all references in the ABL4 range
MTBF according to standard SN29500 is >500000 hours
MTBF according to MIL Std HDBK217F is >150000 hours
Gepubliceerd voor:Schneider Electric Netherlands
Ontdek meer
Ontdek meer