Veelgestelde vragen (FAQ's) zoeken
Why use ABL8PRE24100 and ABL8PRP24100 protection modules associated with the power supplies?
All Phaseo switch mode power supplies incorporate protection of their secondary circuit against overloads and short-circuits. However, it is good practice to use fuses or circuit-breakers in addition to this protection.
These devices are used mainly as isolators when debugging or repairing the machine, but they never trip because the electronic protection built into the power supply is faster.
This means that there is no protection discrimination, and the slightest overload or short-circuit in the control system will result in the test voltage being cut off.
The ABL8PRE24100and ABL8PRP24100 protection modules offer total output protection discrimination for the switch mode power supply.
Protection modules offer the following advantages:
- Truly discriminating protection: an overload or short-circuit on one circuit will not affect the other circuits.
- Easy installation with modules in blocks of 4 channels.
- For easy selection and guaranteed product availability, each channel can be adjusted from 1-10 A on the front panel.
Only 2 product codes:
- An Optimum product, ABL8PRE24100, which offers the basic functions of an electromechanical circuit-breaker (protection, isolation and manual reset) with the added benefit of discrimination.
- A Universal product, ABL8PRP24100, which in addition to the basic functions offers a choice between manual and automatic reset and 2-pole isolation. In addition, the "tripped" data item is available via a volt-free contact for feedback to the PLC.
The choice of power supply depends on the nominal current to be supplied.
Please note: The Optimum product, ABL8PRE24100, is not commercialised in the UK and Ireland markets.