Søk i ofte stilte spørsmål (FAQ)
How do you setup Metasys N2 on the ATV212 Drives?
Issue:
Set up Metasys N2 on the ATV212 Drives.
Product Line:
ATV212 and S-flex
Environment:
All
Cause:
Metasys N2 setup
Resolution:
Controlling Drive with N2 with start stop and speed reference.
FNOD= 4
CNOD= 2
F108 is 0
F807 =1 terminal wiring or 0 for RJ45
F829= 2 N2 setup
F851= 4 network fault setup
F890= 1 thru 3 for addressing
F892= 300 for a 30 sec time out
To start the drive via network.
Binary output point 3 is CMD
Analog output point 1 is speed freq reference
Monitor status and speed
Binary input point 6 is ETA run status
Analog input point 1 is output speed
For monitoring only everything else the same as above.
FNOD= 1 for VIA or the customer can choose.
CNOD= 0 for terminal start stop
F108= 48
Wiring on Terminals
+ is B terminal
- is A terminal
Ground is GND terminal
Shield is SCR terminal