ค้นหาคำถามที่พบบ่อย
Can I change the IP address of the Magelis in Vijeo Designer and download the changes over ethernet?
Issue:
Changing the IP address of the Magelis in Vijeo Designer and download the changes over ethernet
Product Line:
Vijeo Designer
Resolution:
No, It's not possible to change the IP address of the Magelis from Vijeo Designer and still download over ethernet.
To make changes to the IP address, you have to download either via USB cable or file system.
เผยแพร่สำหรับ:ชไนเดอร์ อิเล็คทริค Thailand
ดูข้อมูลเพิ่มเติม
รุ่น:
ดูข้อมูลเพิ่มเติม
รุ่น: