ค้นหาคำถามที่พบบ่อย
Can we upload programs with Vijeo Designer from the Magelis XBTG/GK/GT, HMIGK/GTO/GTU, HMISTO/STU?
Goals and Symptoms
Can we upload programs with Vijeo Designer from the Magelis XBTG/GK/GT, HMIGK/GTO/GTU, HMISTO/STU?
Causes and Fixes
It is necessary to previously configure the Vijeo-Designer project according to: In the Target's properties, for XBTG/GK/GT, HMIGK/GTO/GTU, HMISTO/STU...
- select download File System
- enable the Include Editor Project in the Download property.
In other words: if the project has not been downloaded with this option, you cannot upload it.
เผยแพร่สำหรับ:ชไนเดอร์ อิเล็คทริค Thailand
ดูข้อมูลเพิ่มเติม
รุ่น:
ดูข้อมูลเพิ่มเติม
รุ่น: