ค้นหาคำถามที่พบบ่อย
How do I set the Time of Day(TOD) clock in the SY/MAX PLCs?
Issue
How do I set the Time of Day (TOD) clock in the SY/MAX PLCs?
Product Line
TSX Micro
Environment
Sy/Max
Resolution
To set the TOD clock in a SY/MAX controller first enter a value of "-1" into register 8108, then enter the new values into the remaining TOD clock registers (8109-8115). Finally to update and restart the TOD clock enter a value of "0" into 8108. The following table illustrates the SY/MAX TOD clock registers and their function:
REGISTER | FUNCTION | DECIMAL RANGE |
8108 | SET CLOCK | -1 (set), 0 (normal), 1(stop watch) |
8109 | Seconds | 0-59 |
8110 | Minutes | 0-59 |
8111 | Hours | 0-23 |
8112 | Day of Week | 1-7 (1= Sunday) |
8113 | Day of Month | 1-31 |
8114 | Month | 1-12 |
8115 | Year | 1980-2079 |
เผยแพร่สำหรับ:ชไนเดอร์ อิเล็คทริค Thailand
ดูข้อมูลเพิ่มเติม
รุ่น:
ดูข้อมูลเพิ่มเติม
รุ่น: