ค้นหาคำถามที่พบบ่อย
Bacnet Troubleshooting Tool
If you have a project in Powerlogic scada or Citect in which you have bacnet devices, you can use the "cas-bacnet-explorer" tool for troubleshooting the bacnet devices and to verify your data in PLScada. This tool doesn't use the bacstac service that the Bacnet driver in PLS uses so it is a good tool to use for troubleshooting.
The link below shows some screen caps on how the tool works and there is a training video too. You can download the tool for the same link. The tool will work for couple of hours before it will ask you to purchase the full version.
https://store.chipkin.com/products/tools/cas-bacnet-explorer
Related ranges: PowerSCADA Expert 7.3, PowerLogic SCADA 7.1, PowerSCADA Expert 7.2
เผยแพร่สำหรับ:ชไนเดอร์ อิเล็คทริค Thailand
ดูข้อมูลเพิ่มเติม
รุ่น:
ดูข้อมูลเพิ่มเติม
รุ่น: