ค้นหาคำถามที่พบบ่อย
Is there a document available that shows which roof height adapters are used in various applications like EcoAisle and InRow?
Issue:
There's a need to confirm the correct roof height adapter; that it's compatible with the product and application where it's being installed.
Product Line:
InRow Cooling, NetShelter SX, NetShelter VX
Environment:
All versions and serial ranges.
Cause:
There are a few PDUs which don't have mounting holes for roof height adapters, and there is need to help choose the correct roof height adapter for a particular application.
Resolution:
See attached file
เผยแพร่สำหรับ:ชไนเดอร์ อิเล็คทริค Thailand
เอกสารแนบ
ดูข้อมูลเพิ่มเติม
รุ่น:
ดูข้อมูลเพิ่มเติม
รุ่น: