ค้นหาคำถามที่พบบ่อย
Osisense XM - Routine maintenance of the XML or 9012 pressure switches
Please find attached the maintenance operations relevant to the pressure switches in all the families, including especially the XMLA/B/C/D series and the class 9012 ...
If the customer needs to check periodically the pressure switch adjustment, he can do it with some manometer on the pressure switch circuit. Time between 2 verifications depends on the product mission profile
If the customer needs to check periodically the pressure switch adjustment, he can do it with some manometer on the pressure switch circuit. Time between 2 verifications depends on the product mission profile
เผยแพร่สำหรับ:ชไนเดอร์ อิเล็คทริค Thailand
เอกสารแนบ
ดูข้อมูลเพิ่มเติม