ค้นหาคำถามที่พบบ่อย
Galaxy 5000, Galaxy 5500; Dust Covers
Issue:
It has been determined that dust and other foreign conductive particles have been getting inside the UPS during shipping or from site construction projects during installation.
Product line:
Galaxy 5000, Galaxy 5500
Environment:
All models, all serial numbers
Cause:
Conductive dust and particles negatively affect system operation by increasing component temperatures and reducing dielectric strength.
Resolution:
Temporary front and top covers are being applied to Galaxy 5000 units prior to shipping to protect the unit from foreign particles.
FRONT dust protection cover
TOP dust protection cover
Only Schneider Electric Certified Field Service Engineers are authorized to remove this cover.
Bottom Portion can be lifted to provide access to input / output wiring section.
เผยแพร่สำหรับ:ชไนเดอร์ อิเล็คทริค Thailand
ดูข้อมูลเพิ่มเติม
รุ่น:
ดูข้อมูลเพิ่มเติม
รุ่น: