ค้นหาคำถามที่พบบ่อย
What is virtual injector in Easergy P3 and how to activate the virtual Injector?
The virtual injector will feed samples to the hardware inputs.
Virtual injector can only be activated when you are connected to the device and logged in as configurator. A green left arrow appears in upper right corner and by selecting that the virtual injector configuration screen appears and you can select "Activate virtual injections".
The device will trip for any function activated which exceed the threshold setting and the outputs connected will be activated. There is no setting to prevent an activation specific for virtual injection.
Virtual injector can only be activated when you are connected to the device and logged in as configurator. A green left arrow appears in upper right corner and by selecting that the virtual injector configuration screen appears and you can select "Activate virtual injections".
The device will trip for any function activated which exceed the threshold setting and the outputs connected will be activated. There is no setting to prevent an activation specific for virtual injection.
เผยแพร่สำหรับ:ชไนเดอร์ อิเล็คทริค Thailand
ดูข้อมูลเพิ่มเติม
รุ่น:
ดูข้อมูลเพิ่มเติม
รุ่น: