ค้นหาคำถามที่พบบ่อย
What are the meaning of DM, PrsDM, PrdDM and MD of PM2100
The parameter in the yellow circle:
DM Last Demand
PrsDM Present/ Raising demand
PrdDM Predictive demand
MD Max Demand
Power Demand
Power demand is a measure of average power consumption over a fixed time interval.
NOTE: If not specified, references to “demand” are assumed to mean “power demand.”
The meter measures instantaneous consumption and can calculate demand using various methods.
Current demand
The meter calculates current demand using the block interval, synchronized or thermal demand methods.
You can set the demand interval from 1 to 60 minutes in 1 minute increments (for example, 15 minutes).
Predicted demand
The meter calculates predicted demand for the end of the present interval for kW, kVAR, and kVA demand, taking into account the energy consumption so far within the present (partial) interval and the present rate of consumption. Predicated demand is updated according to the update rate of your meter. The following illustration shows how a change in load can affect predicted demand for the interval. In this example, the interval is set to 15 minutes.
เผยแพร่สำหรับ:ชไนเดอร์ อิเล็คทริค Thailand
ดูข้อมูลเพิ่มเติม
รุ่น:
ดูข้อมูลเพิ่มเติม
รุ่น: