ค้นหาคำถามที่พบบ่อย
What is the tightening torque recommended to be applied for fixing the Masterpact NW devices to the mounting plate?
Masterpact NW circuit breakers and switch disconnectors may be installed in various switchboards and horizontal mounting plates. Each system has its own installation method of these breakers and the tightening torque needs to be adapted by the panel builder considering the screw size. The mounting plate is horizontal and the role of those bolts and nuts is to avoid circuit breaker movement.
Nevertheless, the torque usually applied on such M8 class 8.8 bolts and nuts is < 25Nm.
Nevertheless, the torque usually applied on such M8 class 8.8 bolts and nuts is < 25Nm.
เผยแพร่สำหรับ:ชไนเดอร์ อิเล็คทริค Thailand
ดูข้อมูลเพิ่มเติม
รุ่น:
ดูข้อมูลเพิ่มเติม
รุ่น: