ค้นหาคำถามที่พบบ่อย
Where is the position to install Auxiliaries on EasyPact CVS?
All EasyPact CVS100/160/250 circuit breakers and switch-disconnectors have slots for the electrical auxiliaries listed below.
5 indication contacts
- 2 ON/OFF (OF1 and OF2)
- 1 trip indication (SD)
- 1 fault-trip indication (SDE)
- 1 earth-fault indication (SDV), when the device is equipped with a Vigi module.
1 remote-tripping release
- either 1 MN undervoltage release
- or 1 MX shunt release.
All these auxiliaries can be installed with a rotary handle.
All EasyPact CVS400/630 circuit breakers and switch-disconnectors have slots for the electrical auxiliaries listed below.
6 indication contacts
- 3 ON/OFF (OF3)
- 1 trip indication (SD)
- 1 fault-trip indication (SDE)
- 1 earth-fault indication (SDV), when the device is equipped with a Vigi module.
1 remote-tripping release
- either 1 MN undervoltage release
- or 1 MX shunt release.
All these auxiliaries can be installed with a rotary handle.
The illustration shown (TMD, MA, NA and ETS 2.3 standard) indicates auxiliary possibilities depending on the type of trip unit.
5 indication contacts
- 2 ON/OFF (OF1 and OF2)
- 1 trip indication (SD)
- 1 fault-trip indication (SDE)
- 1 earth-fault indication (SDV), when the device is equipped with a Vigi module.
1 remote-tripping release
- either 1 MN undervoltage release
- or 1 MX shunt release.
All these auxiliaries can be installed with a rotary handle.
All EasyPact CVS400/630 circuit breakers and switch-disconnectors have slots for the electrical auxiliaries listed below.
6 indication contacts
- 3 ON/OFF (OF3)
- 1 trip indication (SD)
- 1 fault-trip indication (SDE)
- 1 earth-fault indication (SDV), when the device is equipped with a Vigi module.
1 remote-tripping release
- either 1 MN undervoltage release
- or 1 MX shunt release.
All these auxiliaries can be installed with a rotary handle.
The illustration shown (TMD, MA, NA and ETS 2.3 standard) indicates auxiliary possibilities depending on the type of trip unit.
เผยแพร่สำหรับ:ชไนเดอร์ อิเล็คทริค Thailand
เอกสารแนบ
ดูข้อมูลเพิ่มเติม
รุ่น:
ดูข้อมูลเพิ่มเติม
รุ่น: