ค้นหาคำถามที่พบบ่อย
How can I define the communication period of my PowerTag Energy Sensor ?
Communication for PowerTag Energy Sensor is set by default to 5 seconds in wireless gateway. But to decrease Wireless traffic it is recommended to increase this value according to Edge Control system needs (PLC, SCADA…).
Example: It is not usefull that the wireles gateway requests metering data for PowerTag Sensor every 5 seconds if SCADA requests only each 30 seconds the wireless gateway.
Example: It is not usefull that the wireles gateway requests metering data for PowerTag Sensor every 5 seconds if SCADA requests only each 30 seconds the wireless gateway.
เผยแพร่สำหรับ:ชไนเดอร์ อิเล็คทริค Thailand
ดูข้อมูลเพิ่มเติม
รุ่น:
ดูข้อมูลเพิ่มเติม
รุ่น: