ค้นหาคำถามที่พบบ่อย
How do Automations work in Wiser system?
Automations in our system are working with triggers, they will start only after a status change. They will not take into account the previous values.
You can Start the new Automation by the example below:
- (See A) On the Home page, tap the
icon.
- (See B, C) On the Moment page, tap the Automation tab (B) and then tap the + icon (C).
- (See D, E) Set a name for the Automation (for example, Welcome) (D) and optionally a background image (E).
An Action is required to operate the light switch, shutter, and dimmer devices in the Living Room. Configure the Action by setting one or more Tasks.
NOTE: This example shows the setting of the light switch.
- (See A) Tap Add Task.
- (See B) Tap Run the device. There are four types of tasks and these can be added to the action list in Automation.
- (See C) Select the Living Room light switch from the list.
- (See D, E) Select the Switch (D) and set its state to On (E).
- Tap Save, then Next.
(See F) The switch Task is displayed in the Action section of the Automation page.
TIP: If you want to delete a created action, swipe the action to left and tap the Delete option. To re-order the existing actions, tap and hold action and drag it to the desired position in the list. - Add further Tasks to set Shutter open (G) and Dimmer level (H)
At least one Condition is required to trigger an Automation.
NOTE: For this example, a Condition will be set to trigger the Automation when the front door is opened and the motion sensor (installed externally) is detecting the movement. This involves selecting the front door Window/Door sensor and selecting the motion sensor. Also, choosing the Open and motion detected Condition.
- (See A) Tap Add Condition.
- (See B) Tap When device status changes.
- (See C) Select the Front Door Window/Door Sensor.
- (See D) Tap the Window/Door Sensor function.
- (See E) Select the Open condition.
- The Window/Door Sensor is displayed in the Condition section of the Automation page.
Repeat the steps from 1 to 6, to add the conditions to trigger the automation for Motion Sensor. Both devices are now displayed in the Condition section of the Automation page (see F). - (See G) For Automations with more than one condition, set whether the Automation should be triggered when any condition is met, or only when all conditions are met.
You have a choice to trigger the automation when any or all conditions are met. However, in this case, the automation is triggered when all the conditions are met.
TIP: In case you want to delete a created condition, then, swipe the condition to left and tap the Delete option. - If you want to limit to when this automation occurs, for ex, between 6-7pm when arriving from work, then tap Effective Period field in the app and set a time interval.
- (See H) Tap Save.
The finished Automation (I) is displayed on thepage under the Automation tab.
Tap the Enable switch (J) on the Automation button to enable/disable the Automation. Tap the Edit (...) icon (K) to change the Automation settings.
You can find this and more details in our Wiser System User Guide.
เผยแพร่สำหรับ:ชไนเดอร์ อิเล็คทริค Thailand
ดูข้อมูลเพิ่มเติม
ผลิตภัณฑ์:
ดูข้อมูลเพิ่มเติม
ผลิตภัณฑ์: