我们今天能为您提供什么帮助?

Modbus Register Maps for APC by Schneider Electric Rack PDU's

Issue:
Looking for Modbus Register Maps for APC by Schneider Electric Rack PDU's

Product:
APC by Schneider Electric Rack Mountable PDU's with part numbers beginning with AP88XX, AP89XX, AP78XXB, AP79XXB, APDU99XX, APDU11XXXX, EPDU1XXXX, EPDU2XXXX

Solution:

Most APC Rack PDUs support Modbus over TCP. However, units equipped with first-generation Network Management Cards (NMC1) do not include Modbus functionality.

Modbus support is available on:

  • Rack PDUs with NMC2 running firmware version 6.x.x or higher
  • All Rack PDUs based on NMC3 technology

Important Note: The APDU10XXXX Advanced Rack PDU series does not use NMC3 technology and therefore does not support Modbus. This series has been replaced by the APDU11XXXX variant, which incorporates NMC3 and provides full Modbus functionality.

How to locate the correct Modbus Register maps for your device:


Step 1:
Visit https://www.se.com/ and select your country.
Note: Available units and documentation may vary by region.The following image shows where to find the country selection

Step 2:
From the main menu, go to SupportProduct Documentation & SoftwareAll Documents and Software.
The following image shows the menu to access to find the documents for Modbus


Step 3:
In the search box, enter PDU Modbus or Easy PDU Modbus, depending on your device.
This will display all relevant documents available for download.
The following image shows all docs for APC NMC based PDU's

The following image shows all docs for APC Easy Brand PDU's

If you have any clarifications or concerns, please do contact us at 1-800-800-4272 or chat with our Technical Support Agents.

Schneider Electric Rack PDU's | 施耐德電機Taiwan