Чим ми можемо вам допомогти сьогодні?

How to configure the communication between a BMENOP0300 module and an C264 device ?

To configure a C264 device, we use the PACIS SCE tool to generate a ZIP configuration file, which is then transferred to the C264 device using another software called PACIS CAT.

It is mandatory to use this same ZIP file to configure the BMENOP0300 module, by extracting the .SCD configuration file from it and using the Modicon IEC61850 Configuration tool to transfer it to the module.

schema