Features
Magelis GTU is the first smart-phone-like HMI with resistive multi-touch screen without screen size limitation powered by Vijeo XD. The last novelty is the innovative Magelis GTU Wireless LAN display with access point and station mode*.
Magelis GTU ensures high level of performance and openness:
*Depending on the environment, the location to the GTU screen (distance and angle) as well as the used application.
Benefits
Applications
- Complex machines
- Food and beverage, water, waste water, minning, mineral, metal
- Packaging, conveying