Søk i ofte stilte spørsmål (FAQ)
What is the part number for a replacement knob on ATV61/71/212 keypad, VW3A1101?
Issue:
Replacement part number for knob on ATV61/71/212 keypad, VW3A1101.
Product Line:
VW3A1101 Keypad
Environment:
All model numbers.
Cause:
The main knob has broken off or is missing and a replacement is needed. The keypad still works properly, only the knob is missing.
Resolution:
There is no part number to order a replacement knob.
If the keypad was manufactured prior to Week 22 of 2012 then US customers can reach out to drive.products.support@schneider-electric.com to see if any replacement knobs remain available.
Be sure to include a shipping address and the serial number from the keypad (found on the label on the back of the keypad).
Publisert for:Schneider Electric Norway
Finn ut mer
Finn ut mer