ค้นหาคำถามที่พบบ่อย
Creating Kernel Dumps for PowerLogic Scada and PowerScada Expert
Steps for getting the kernel dump files:
- Make sure you have a User Named Kernel with password kernel in Project Editor with Roles set as ES_Admin.
- Open Powerlogic Scada Runtime Manager. Highlight the Process you want to take the kernel dump for, right click on it and select kernel.
-
- - The kernel window will open as shown below. Then go to tools then click on Reset Stats
-
- - Then go to View and click on Cicode. Then it will ask you for the password. The password is kernel.
-
- - After typing the password, a new window will open in which you type in it the function dumpkernel(0xC000,) and click enter. The return value should be 0 as shown below.
-After you have done this for all the I/O Servers, Alarm server and trend server your next step will be to copy the created files. You should see a file for each I/O, Alarm and trend Servers
-Navigate to Citect explorer and select View, Log Folder, as shown below: This will take you to the location of the Log Files.
-The files you would need are the ones that are created today with the word Kernel in the beginning of the name and .dat file extension.
Legacy KB System (APS) Data: RESL210836 V1.0, Originally authored by RaDe on 03/02/2013, Last Edited by RaDe on 03/02/2013
Related ranges: PowerSCADA Expert 7.2, PowerLogic SCADA 7.1
เผยแพร่สำหรับ:ชไนเดอร์ อิเล็คทริค Thailand
ดูข้อมูลเพิ่มเติม
รุ่น:
ดูข้อมูลเพิ่มเติม
รุ่น: