Issue
Control power specifications of the various meters
Product Line
Sepam 10, Sepam 20, Sepam 40, Sepam 80, CM2000 (CM2), CM3000 (CM3), CM4000 (CM4), CM4ECC (ECC21), PM1000, PM210 (PM2), PM700 (PM7), PM800 (PM8), PM5000, PM8000, ION6200, ION7300, ION7550, ION7650, ION8600, ION8650, Enercept Meter, Energy Meter, SMD63, EM4805
Environment
Metering application requiring control for the metering devices
Cause
Need to select power supply to power meters
Resolution
The burden ratings for the Powerlogic, ION, and SEPAM devices are outlined in the attached EXCEL spreadsheet.
เผยแพร่สำหรับ: ชไนเดอร์ อิเล็คทริค Thailand