Issue
Need to know what data is logged by default on the PM5500.
Product Line
PM5500 series meters
Environment
Onboard data logs
Cause
Factory default logged values are not known by customer.
Resolution
The PM5500 Series supports onboard logging for up to 14 user-selectable measurements. You can select these measurements as follows:
The device driver polls the device and checks for new log entries at regular intervals. The default polling interval is 30 seconds.
The polling interval can be modified by changing the value of the register "R3 Poll Period Seconds" in ext_pm5500.ion in the …\system\translators folder. The lowest possible polling interval is 5 seconds.
The measurements available for selection are as follows:
เผยแพร่สำหรับ: ชไนเดอร์ อิเล็คทริค Thailand