ค้นหาคำถามที่พบบ่อย
Can the outputs on the VIP410 be customized
Issue
The outputs are pre assigned, but can it be customized.
Product Line
VIP410
Environment
Wiring outputs and inputs.
Cause
Outputs on the VIP410 need to be customized.
Resolution
![Customizing Output Customizing Output](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0151H000008zqN2QAI&oid=00DA0000000abSm)
![block diagram block diagram](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0151H000008zqIJQAY&oid=00DA0000000abSm)
The outputs are pre assigned, but can it be customized.
Product Line
VIP410
Environment
Wiring outputs and inputs.
Cause
Outputs on the VIP410 need to be customized.
Resolution